This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL137 Computing Power

I'm developing on  OMAP-L137 http://www.ti.com/tool/tmdsoskl137

I tried to design my own audio effect. I have FIFO to keep audio data.

FIFO is just a one-dimension array. It's  short[10000] 

(I enlarge stack and heap size.  So, there is no problem to use short[10000])

one FIFO input could work.  

I could retrieve sound from ADC and generate sound to DAC.

"FIFO input" is save data in one-dimension array.

/**** standard sample code  ,  add one FIFO input****/

/*** work successfully ***/

for ( sec = 0 ; sec < 1000 ; sec++ ){
  for ( msec = 0 ; msec < 1000 ; msec++ ){
    for ( sample = 0 ; sample < 48 ; sample++ ){
      /* Read then write the right sample */
      while ( ! ( MCASP1_SRCTL0 & 0x20 ) );
      right_data = MCASP1_RBUF0_32BIT;
      while ( ! ( MCASP1_SRCTL5 & 0x10 ) );
      MCASP1_XBUF5_32BIT = right_data;
      /* Read then write the left sample */
      while ( ! ( MCASP1_SRCTL0 & 0x20 ) );
      left_data = MCASP1_RBUF0_32BIT;
      fifo_input (left_data);
      while ( ! ( MCASP1_SRCTL5 & 0x10 ) );
      MCASP1_XBUF5_32BIT = left_data;
    }
  }
}

/**** standard sample code  ,  add two  FIFO input****/

/*  Can't Work */

for ( sec = 0 ; sec < 1000 ; sec++ ){
  for ( msec = 0 ; msec < 1000 ; msec++ ){
    for ( sample = 0 ; sample < 48 ; sample++ ){
      /* Read then write the right sample */
      while ( ! ( MCASP1_SRCTL0 & 0x20 ) );
      right_data = MCASP1_RBUF0_32BIT;
      while ( ! ( MCASP1_SRCTL5 & 0x10 ) );
      MCASP1_XBUF5_32BIT = right_data;
      /* Read then write the left sample */
      while ( ! ( MCASP1_SRCTL0 & 0x20 ) );
      left_data = MCASP1_RBUF0_32BIT;
      fifo_input (left_data);
      fifo_input (left_data);
      while ( ! ( MCASP1_SRCTL5 & 0x10 ) );
      MCASP1_XBUF5_32BIT = left_data;
    }
  }
}

==>ADC / DAC can't have sound.  It can't work.

Two FIFO input might consume too many CPU operation.

Why?   C6747 should be 375MHz

375000000 / 48000 (sample rate) / 4 (2ADC,2DAC)  = 1953

There should be enough CPU computing power to do "two FIFO input".

How to improve this? Please help me.  Thx!