This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

audio capture problem

Expert 2990 points

Other Parts Discussed in Thread: TLV320AIC32

Hi all:

I encountered a strange problem about audio capture.

I use the command arecord -f cd | aplay to test audio capture and display.

The input source is a notebook,The output source is a small speaker.

First I run the command arecord -f cd | aplay

Then I set the maximum display volume through  amixer cset name="PCM Playback Volume" 100%

The display audio quality is well . 

When I set the maximum capture volume through  amixer cset name="PGA Capture Volume" 100%

The display audio quality is very noisy

So I set the capture volume to 50% through amixer cset name="PGA Capture Volume" 50%

The noise is reduced

Later,I also did a test that

I increased the volume of the input source but not increased the capture volume

The display audio quality is well

So I suspect there may be a problem tlv320aic32