Hi,
I have a question about C6678 DDR3.
If we want to use 8GByte DDR3 memory, how to configure in the C6678?
In the the C6678 datasheet, it seem that we can use up to 8GByte DDR3.
But in page.27 Table 2-2, there is only 2GB address space for DDR3 EMIF data.
I understand as follow, but I don't know it's either correct or not.
* Need to configrure XMC MPAX Segment Registers of MSMC and
for example if using 2 segment and setting each SEGSZ to 4GB,
we could use up-to 8GB. Am I correct?
So, to use 8GByte need to configure more than 2 segment.
Am I correct?
best regards,
g.f.