Dear Expert
When using Generic 16bits yUV mode in DM365, Interrupt is not generated even though data comes at VPFE.
We uses external VSYNC,HSYNC and pixel clock from external ISP device and register setting is like as below.
FMTSPH:0x00000000
FMTLNH:0x00000000
FMTSLV:0x00000000
FMTLNV:0x00000000
FMTRLEN:0x00000000
FMTHCNT:0x00000000
SPH:0x00000000
LNH:0x000004FF
SLV0:0x00000001
SLV1:0x00000001
LNV:0x000003FF
PPLN:0x00000000
LPFR:0x00000000
HSIZE:0x00000000
End of ccdc_setwin...ccdc_config_ycbcr():win(l,t,w,h):(0, 0, 1280, 1024)
ccdc_config_ycbrcr() : params->frm_fmt == CCDC_FRMFMT_PROGRESSIVE
ccdc_config_ycbrcr() : params->buf_type == CCDC_BUFTYPE_FLD_INTERLEAVED
ccdc_config_ycbrcr(): ccdc_if_type == CCDC_YCBCR_SYNC_16
End of ccdc_config_ycbcr...
ccdc_enable(): SYNCEN:0x00000001
ccdc_output_to_sdram(): SYNCEN:0x00000003
Is there any check point or usage note for 16bits YUV interface?.