This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

xds560 plus v2 download problem

Hello ,I'  using ssd xds560 plus v2 emulator under ccs5.2,and when I debug program which using dsp/bios 5.41 ,it will take me about  1 minute to download the program(it's size is about 330KB), but if I don't use dsp/bios 5.41, for example I use sys/bios or without any OS, it will take me only a few seconds to download a problem, what's the problem , can you help me , waitting for your answer, thank you!

  • Hi cz h,

    What hardware platform are you loading your program onto?

    What are the sizes of the other programs (the ones that load quickly)?

    Could you attach the memory maps of each program (the one that is slow to load, as well as the ones that are loading quickly)?

    Steve