I use TI's official color bar test procedures and test ADV7343 driver, the output ADV7343 termination LCD TV, only snow point when you run the program, how is this going?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It might be getting disabled. it is a setting of adv7343. just look into the driver and see where it is getting disabled.
Hi,
I think you were asking about why color bar is getting stopped. there is a configuration in adv7343 to enable/disable internal color bar. But disabling color bar does not stop the output, it will still output untill output is really stopped.
Regards,
Brijesh
Hi,
yes, im sure there is a right configuration in adv7343 to enable internal color bar .
adv7343 1-002a: chip found @ 0x54 (DaVinci I2C adapter)
ADV7343 REG 0x00 val = 12
ADV7343 REG 0x01 val = 0
ADV7343 REG 0x02 val = 20
ADV7343 REG 0x80 val = 14
ADV7343 REG 0x82 val = 9b
ADV7343 REG 0x83 val = 4
ADV7343 REG 0x84 val = 70
ADV7343 REG 0x86 val = 2
ADV7343 REG 0x87 val = 2f
ADV7343 REG 0x88 val = 20
ADV7343 REG 0x89 val = 0
ADV7343 REG 0xA0 val = 7f
ADV7343 REG 0x99 val = 10
ADV7343 REG 0xA1 val = 3
ADV7343 REG 0x17 val = 0
but TV show like that:
Regards,
alvin
So What's the issue? Are these artifact on tv issue? Can you make sure you input is correct?
Regards,
Brijesh