We are in phase of redesign our DM3730 custom board and want to add support of eMMC via MMC2 interface.
Could you be kind to comment some my questions"
1) Connection seems simple. Connect direct MMC2 lines to EMMC ?
eMMC control lines are also 1V8 compatible.
2) Connect VCC (memory part of eMMC) to +3V3 (available)
3) I am a little confused with MMC2 boot and MMC2_H.
What is difference? For example, we already use MMC1 for SD card (3V3)
What we really need to do ? Connect VDDS_MMC1 (which is 3V) to memory part of
eMMC or something other? It should be optional , but I want to provide.
Thank in advance