This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does hyperlink play the same role as TeraNet on C6678?

Hi,all:

I see the figure in the  datasheet of C6678  sprs691d.

1.

From the figure,It seems that Hyperlink play the same  job as TeraNet. Doesn't it?

it seems that TeraNet and Hyperlink can be considered as common Bus.

All cores including core0-core7 also can switch data via common Bus.

Doesn't it?

Please correct me If I miss anything.

2.

If above so, Can corepacs (such as core0 and core1) transfer data via Hyperlink like TeraNet?

3.

Can corepacs(such as core0 and core1) transfer data via PCIE like TeraNet?