This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730CUS 512MB LPDDR

Other Parts Discussed in Thread: DM3730

Our current DM3730CUS prototype uses 1 256MB 32-bit LPDDR400 chip.  This has worked well.  Now I need to double the amount.  I was planning on just adding the same 32-bit part on the second chip select (cs1) and second clock enable (cke1).  Part is MT46H64M32LFCX-5 IT:B.  We went ahead and routed Data, Address, etc on a T network with each branch of the network being length matched per the datasheet.  Termination resistors are right next to the DM3730 and so are the DRAM chips, Overall trace lengths are around 2.7 inch at most, so this is pretty compact.  The layout guidelines don't really talk about a second chip on the other chip select so I'm assuming we did the right thing?  For example, Figure 6-22 isn't too helpful because it looks like this figure is for two 16-bit devices.  Can someone please confirm we did the right thing here for layout and DRAM compatibility.

Thanks