Hi
I am looking for information about memory performance in the C6678 DSP.
I understood that:
MSMC SRAM has 4 memory banks of 256 bits, and all 4 banks can be accessed simultaneously by separate cores or other system masters.
But in the Application Report Throughput Performance Guide for C66x KeyStone Devices(SPRABK5A1)
5.3 Scenario 3: EDMA Transfer From MSMC SRAM to MSMC SRAM,
I found the following description:
"so there is only one transfer happening at a time. "
"it cannot do both reads and writes at the same time."
Is that contradiction?
Which is correct?
Or I misunderstood it?
Thank you.
Yin