Other Parts Discussed in Thread: OMAP-L137
when OMAPL137 connect ksz8893 ,how to configure the OMAPL137 and ksz8893 ,then I can use two Internet port to communicate with the pc,can you give me something to comprehensive it .
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L137
when OMAPL137 connect ksz8893 ,how to configure the OMAPL137 and ksz8893 ,then I can use two Internet port to communicate with the pc,can you give me something to comprehensive it .
Xuewu Peng,
KSZ8893:
Integrated 3-Port 10/100 Managed Switch with PHYs.
Find the network oriented examples (requires Ethernet) at the NDK package like ndk_2_0_0
Ethernet Interface:
The OMAP-L137 incorporates an ethernet MAC which interfaces to a Micrel KSZ8893MQL ethernet switch. The multi-port 10/100 Mbit interface is isolated and brought out to two RJ-45 standard ethernet connectors, P9, P10.
Please see the EVMOMAPL137_TechRef for the interface.
You can find the EMAC, setmac test code at the EVMOMAP-L137 BSL package.
http://support.spectrumdigital.com/boards/evmomapl137/revg/files/revg_EVMOMAPL137_BSL.zip
In addition that, refer the sections "Functional Description and Overview".
Find the more details for how to configure the switch at the datasheet.
http://support.spectrumdigital.com/boards/evmomapl137/revd/files/micrelksz8893MQL.pdf