Dear,
I have compile problem when I try to compile the GoDB UI of IPNC
After download GoDB IDE from the GoDB website according to IPNC WEB UI Code Guide.pdf, when i compile the project, there are 27 build errors without any modification. ( Just I want to replace the login background image. )
Most of all, when I compress gIPNC-ro.bdb to gIPNC-ro.gz, the command console is crashed and there is no output files. My build system is Windows XP.
are they incomplete source?
Best regards
Aden Yoon