Other Parts Discussed in Thread: DM385
Hi !
I'm in trouble for DM385 SD booting.
I got below message.
I guess, PGM is not workinng in DDR .
May I have some advices?
-------------------------------------------------------------------
U-Boot 2010.06 (Dec 13 2013 - 10:55:52) DM385_IPNC_3.50.00
DM385-GP rev 1.1
ARM clk: 600MHz
DDR clk: 533MHz
L3 clk: 200MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP Default OFF
DSS Default OFF
DRAM: 1 GiB
MMC: OMAP SD/MMC: 0, ON-BOARD SDIO: 1
Using default environment
The 2nd stage U-Boot will now be auto-loaded
Please do not interrupt the countdown till DM385_IPNC prompt if 2nd stage is already flashed
Hit any key to stop autoboot: 0
reading u-boot.bin
199432 bytes read
## Starting application at 0x80800000 ...
-------------------------------------------------------------------