Hello,
My customer is faceing a problem with AM3352 processor with NAND256W3A0BZA6 attached.
Could you help to configure the GPMC module to work properly with above NAND Flash.
Issue is that CS signal needs to be in Active state since command is send until the data is valid.
Since now customer couldn't configure memory controller to do so.
As workaround CS signal is connected to GPIO, it works but it's not a proper solution.
Could you give me some hints, or examples how to configure memory controller?
thanks in advance
MK