Other Parts Discussed in Thread: OMAPL138, OMAP-L138
Hi All,
We have already used OMAPL138 device with NOR flash in our customized board.
We are using sfh_OMAP-L138.exe utility to download UBL and u-boot.bin file to NOR flash and we are successfully able to do that.
But our concern is when we are using the same method to program UBL and u-boot.bin in NAND flash using sfh_OMAP-L138.exe utility, we are not able to do it.
Observation:-
Transfer over UART 100%.
Programming UBL into Flash it get stuck here.
Regards
Rishabh Jain