Anyone can tell me below log msg was due to what wrong..?
My application was used two TI EVM to do video transmit
EVM TX
Aanlog IN==>H.264 Encoder==>USB==>WIFI Module
EVM RX
WIFI Module==>USB==>H.264 decoder==>Analog out
below msg ouput at EVM RX
ref ys
Recv start:expect 1227147
This is WLANRecv-videofile.Recv start:expect 1215874
This is WLANRecv-videofile.WLANLoader_getFrame
[0] @ 0x443c72fe (0x87ad02fe phys) numBytes 123145 (123145) useMask 0 (1)
ref ys
Recv start:expect 1225431
This is WLANRecv-videofile.Recv start:expect 1209503
This is WLANRecv-videofile.Recv start:expect 1208055
This is WLANRecv-videofile.WLANLoader_getFrame
BulkIn IRP Pending!!!
musb_host_rx 1696: RX1 dma busy, csr 2003
BulkIn IRP Pending!!!
BulkIn IRP Pending!!!
BulkIn IRP Pending!!!
BulkIn IRP Pending!!!
BulkIn IRP Pending!!!