This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ice_v2Mux

Hi we are using SDK 1.1.0.3 on ICE Board

what is the difference between this two boards

 AM335X_BOARD_TYPE_ICE_V2 and

AM335X_BOARD_TYPE_ICE

  • Hi we are using SDK 1.1.0.3 on ICE Board what is the difference between this two boards AM335X_BOARD_TYPE_ICE_V2 and AM335X_BOARD_TYPE_ICE

  • Hi,

    Main difference is ICE v2 has support CPSW ethernet ports as well as PRU MII ethernet ports (muxed)

    NOR flash address space access up to 512KB (128KB of ICE v1) without using additional GPIOs.

    There are some changes LED usage (reduced)

    Address selector based on rotary switch and passive matrix LCD support added

    Unlike ICE v1, ICE v2 can directly boot from Micro SD card

    USB connector used for serial console and JTAG is changed to micro (from mini) type

    Changes in certain SPI peripherals (chipselect and SPI instance) connection to AM335x

    For details refer to H/W userguide and schematics

    ICE v1 block diagram

    ICE v2 block diagram