The revE datasheet says to leave the Vpp pins unconnected, but eval board has them connected to 1.8V. Which is correct?
We're not using USB on the 66AK2H12. I was told early that VDDUSB, VP, VPH, VPTX and DVDD33 pins can be connected to GND for this use case. Is this still correct?
Is there any special filtering requirements on the VNWAx pins (fixed Nwell supply), or can these be tied directly to CVDD1, per the eval board?
When will the Hardware Users Guide be available for the 66AK2H12?
thanks,
Scott