Other Parts Discussed in Thread: UCD9222, UCD7242
I need to know what the maximum current draw of VDDT1 is when the Hyperlink bus is disconnected (or idle).
In another post I found, I saw a table for the C6657 (VDDT1 is 65mA max), but this is maximum operating current... I need maximum idle current.
A little background here - we accidentally used a 3.5mil trace to connect the filtered power to the seven (7) VDDT1 pins of the C6678. I need to know if we're going to burn up this tiny trace even though we aren't actually using Hyperlink.
Thanks!
-Bill