hello,
Is it possible to interface camera module with TMS320C5535 DSP??
If possible then please suggetst me the procedure for interfacing that module..
thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
Is it possible to interface camera module with TMS320C5535 DSP??
If possible then please suggetst me the procedure for interfacing that module..
thanks in advance
Yes, there is application interfacing video image to C55 products via the I2S bus and using the SPI to send control signals. The procedure is not avaliable for free. You can match your camera image requirements with the interfaces avaliable on C5535. I2S is a good start to begin with.
Hope this help.
hello steve,
Thanks for responding to my query.Where can i find the procedure for interfacing camera module.??? If it costs some amount i can pay..but i need that..
hello @steve tsang
Please reply to my query soon..submission date is near and i need to complete my project
it's possible or not.....????????
how to interface camera with tms320c65535ezdsp kit........
please explain brief answer ...........
previous answer is not understand.....
so pleas give me your answer.........
Please ask your question in a new post, because this post is marked " Verified Answer" , so these posts are not tracked.