This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Assembly optimization not giving result as expected



Hello all.

I am optimizing the following function in assembly where the height and width is fixed at 2 in the assembly code. I have compared the cycle count, the cycles of the assembly function are significantly less than the C Function when called for a 2x2 block. The cycle count was taken in CCS 3.3 with the clock in profile menu. The assembly code is for davinci Dm6467

 

void mc_chroma( unsigned char *src , int32_t i_src_stride , unsigned char *dst , int32_t i_dst_stride,  int32_t mvx , int32_t mvy , int32_t i_width , int32_t i_height )

{

   unsigned char *srcp;

    int32_t x, y;

    const int32_t d8x = mvx&0x07;

    const int32_t d8y = mvy&0x07;

    const int32_t cA = (8-d8x)*(8-d8y);

    const int32_t cB = d8x    *(8-d8y);

    const int32_t cC = (8-d8x)*d8y;

    const int32_t cD = d8x    *d8y;

    src  += (mvy >> 3) * i_src_stride + (mvx >> 3);

    srcp = &src[i_src_stride];

    for( y = 0; y < i_height; y++ )

    {

        for( x = 0; x < i_width; x++ )

        {

            dst[x] = ( cA*src[x]  + cB*src[x+1] + cC*srcp[x] + cD*srcp[x+1] + 32 ) >> 6;

        }

        dst  += i_dst_stride;        

        src   = srcp;

        srcp += i_src_stride;

    }

}

the assembly for the function is as follows

;;********************************************************************

 

        .global _asm_mc_chroma

        .text

_asm_mc_chroma:

        AND.D1      A8,0x07,A31           ;; d8x = mvx&0x07 

 

||      AND.L2      B8,0x07,B31           ;; d8y = mvy&0x07

||      SHR.S2      B8,3,B9             ;; mvy >> 3

||      SHR.S1      A8,3,A9             ;; mvx >> 3

||      CMPGT.L1    A10,4,A0            ;; A0 = 1 Width 8

||      MVK.D2      0,B2

        SUB.S1      8,A31,A30           ;; 8-d8x

||      SUB.S2      8,B31,B30           ;; 8-d8y

||      MPY.M2      B9,B4,B9            ;; (mvy >> 3) * i_src_stride

||      MV.D1X      B4,A3

||[!A0] CMPEQ.L2    A10,4,B2

        MPY.M2X     A31,B30,B29           ;; cB = d8x    *(8-d8y)

||      MPY.M1X     A30,B30,A29           ;; cA = (8-d8x)*(8-d8y)

        ADD.L1X     B9,A9,A9            ;; (mvy >> 3) * i_src_stride  + (mvx >> 3)

||      ADD.D1      A3,A3,A3            ;; Double Sourece Stride

||      MPY.M2X     A31,B31,B28           ;; cD = d8x    *d8y

        MPY.M1X     A30,B31,A28           ;; cC = (8-d8x)*d8y

||      ADD.D1      A4,A9,A4            ;; src  += (mvy >> 3) * i_src_stride + (mvx >> 3);

||      ADD.L1      A4,A9,A2            ;; Save copy of source pointer

||      MVKL.S1     0x01010101,A24

||      MVKL.S2     0x01010101,B24

||      MV.L2       B4,B2

        MVKH.S1     0x01010101,A24

||      MVKH.S2     0x01010101,B24

||      MV.L1       A6,A1

||      LDNDW.D1    *A4++(A3),A17:A16       ;; Load ROW 1 8-bytes

||      ADD.L2X     A4,B4,B5            ;; Adjusted Pointer for next row

||      ADD.D2      B4,B4,B4            ;; Double Sourece Stride

        MV.L1       B10,A0

||      LDNDW.D2    *B5++(B4),B17:B16       ;; Load ROW 2 8-bytes

||      MPY32.M1    A24,A29,A31           ;; created cA,cA,cA,cA

||      MPY32.M2    B24,B29,B31           ;; created cB,cB,cB,cB

        LDNDW.D1    *A4++(A3),A19:A18       ;; Load ROW 3 8-bytes

||      MPY32.M1    A24,A28,A30           ;; created cC,cC,cC,cC

||      MPY32.M2    B24,B28,B30           ;; created cD,cD,cD.cD

        LDNDW.D2    *B5++(B4),B19:B18       ;; Load ROW 4 8-bytes

||      SHR.S1X     B6,2,A5             ;; created stride for dest stride

;;;;;;;;;;;;;;;;;;;;;;;; 2x2 ;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;;

       LDNDW.D1    *A4++(A3),A27:A26       ;; Load ROW 5 8-bytes

       SHR.S1      A16,8,A17

CHROMA_W2:  

       MPYUS4.M1   A16,A31,A21:A20         ;;1 d1*cA,c1*cA,b1*cA,a1*cA

||     MPYUS4.M2X    A17,B31,B21:B20         ;;1 d1*cB,c1*cB,b1*cB,a1*cB2

||     MVKL.S1     0x00200020,A3         ;; moved low bytes of 32:32

||     SHR.S2      B16,8,B17

       MPYUS4.M1X    B16,A30,A23:A22         ;;1 d2*cC,c2*cC,b2*cC,a2*cC

||     MPYUS4.M2   B17,B30,B23:B22         ;;1 d2*cD,c2*cD,b2*cD,a2*cD

||     MVKH.S1     0x00200020,A3         ;; moved high bytes of 32:32

       MPYUS4.M1X    B16,A31,A21:A20         ;;2 d2*cA,c2*cA,b2*cA,a2*cA

||     MPYUS4.M2   B17,B31,B21:B20         ;;2 d2*cB,c2*cB,b2*cB,a2*cB

||     SHR.S1      A18,8,A19

       MPYUS4.M1   A18,A30,A23:A22         ;;2 d3*cC,c3*cC,b3*cC,a3*cC

||     MPYUS4.M2X    A19,B30,B23:B22         ;;2 d3*cD,c3*cD,b3*cD,a3*cD

       ADD2.D1X    A20,B20,A24           ;;1 ADD cAb1:cAa1 + cCb2:cCa2

||     MVK.S1      0,A2

       ADD2.D2X    A22,B22,B24           ;;1  ADD cBc1:cBb1 + cDc2:cDb2

||     ADD2.D1     A24,A3,A24            ;;1 Added 32  

||     SHR.S1      B6,1,A9

LOOP_chroma_Hi4:

       ADD2.D1X    A24,B24,A24           ;;1 aded the result of row1

||     SHR.S1      A26,8,A27

||     SUB.L1      A0,2,A0

||     SHR.S2      B18,8,B19

       ADD2.L1     A20,A22,A28           ;;2 ADD cAb2:cAa2 + cCb3:cCa3

||     ADD2.D2     B20,B22,B27           ;;2 ADD cBc2:cBb2 + cDc3:cDb3

||     SHR2.S1     A24,6,A24           ;;1 shift right by 6

||     MPYUS4.M1   A18,A31,A21:A20         ;;3 d1*cA,c1*cA,b1*cA,a1*cA

||     MPYUS4.M2X  A19,B31,B21:B20         ;;3 d1*cB,c1*cB,b1*cB,a1*cB2

||[A0] B.S2        LOOP_chroma_Hi4

       ADD2.D1     A28,A3,A28            ;;2 Added 32

||     SPACKU4.S1  A2,A24,A25            ;;1 packed result

||     MPYUS4.M1X  B18,A30,A23:A22         ;;3 d2*cC,c2*cC,b2*cC,a2*cC

||     MPYUS4.M2   B19,B30,B23:B22         ;;3 d2*cD,c2*cD,b2*cD,a2*cD

||[!A0]B.S2      B3

       STH.D1      A25,*A6++[A9]         ;;1 stored first row

||     ADD2.L2X    A28,B27,B27           ;;2 added the results of row 2

||     MPYUS4.M1X    B18,A31,A21:A20         ;;4 d2*cA,c2*cA,b2*cA,a2*cA

||     MPYUS4.M2   B19,B31,B21:B20         ;;4 d2*cB,c2*cB,b2*cB,a2*cB

       SHR2.S2     B27,6,B27           ;;2 shift right by 6

||     MPYUS4.M1   A26,A30,A23:A22         ;;4 d3*cC,c3*cC,b3*cC,a3*cC

||     MPYUS4.M2X    A27,B30,B23:B22         ;;4 d3*cD,c3*cD,b3*cD,a3*cD

       SPACKU4.S1X   A2,B27,A27            ;;2 packed result

||     ADD2.D2X    A20,B20,B25           ;;1 ADD cAb1:cAa1 + cCb2:cCa2

       STH.D1      A27,*A6++[A9]         ;;2 stored first row

||     ADD2.D2X    A22,B22,B24           ;;1  ADD cBc1:cBb1 + cDc2:cDb2

||     ADD2.L1X    B25,A3,A24            ;;1 Added 32 

       NOP

    .end

this function consumes a lot of percentage in the program that I am running and I was expecting that assembly optimization will give me a lot of gain but their is none, I am stumped as to why their is no gain being recieved
thank you in advance
best regards
umair

 

  • The following two statements are saying opposite things.

    Umair Razzak said:

    I have compared the cycle count, the cycles of the assembly function are significantly less than the C Function when called for a 2x2 block.

    ...

    I was expecting that assembly optimization will give me a lot of gain but there is none, I am stumped as to why there is no gain being recieved

    From the first statement it would seem that there is significant gain being received.

    Do both C and assembly give you the exact same results?

    Have you compared the C compiler's assembly output with your assembly file?

  • Well I found out that the calls to the assembly function were less than the calls to the C function. Secondly when comparing the gain I was not comparing the total cycles of the two code variations, as this piece of code is part of a video decoder I was measuring the increase in fps which was almost none. But measuring the cycles (and making sure all the C function calls were replaced) I found out that their was indeed gain it could not be seen as an increase in fps as this snippet of code is not able to significantly improve the fps when optimized.

    thank you for your feedback RandyP and sorry to reply so late.

    best regards

    umair