Hi ,everyone , Happ y Christmas Eve
I follow the guide when prepare the sd , I don't have MIPI display ,I use the DVI display instead. but it don't work ,can you tell me what files is playing a very important role in the card ,so that I can check whether is the error of the sd.
I see the /var/log/dmesg ,but it has nothing , I see the sd ,it has kernel file,and the four switch1010 ,is there some request about the point time of the power then I view the sd/rootfs/boot, I find nothing ,is I do something wrong when I prepare the sd
thank you every much