This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using C6638 K2K, AIF2 "500 us" AT event.

Hi,

I am using the c6638 k2k kelper evm board.

Using the AIF2 driver , my target is to send/receive I&Q samples every 500 us.

For that I am using the pre - defined AT Timer event "5". I am facing issues like

in every 120 milli sec i should get 240 LTE frames but they are coming out to be 298.

Even using the breakpoint in the 500 ms Interrupt isr, clock ticks are around 1600 which is morethan 1 milli sec.

 

Can you please help me in calculating the time interval between 500 us interrupts.

 

Thanks and Regards,

Manav