Hi,
I have a question about NOR FlashWriter for DM6446.
I'm using NOR FlashWriter which is included in "DM644x_FlashAndBootUtils_2_00".
When I try flashing u-boot to the NOR Flash on DM6446EVM, u-boot was flashed successfully.
But when I try with custom board, NOR write Failed.
NOR Flash on custom board is 32MB(part number: JS28F256P30TF)
but EVM's NOR is 16MB(part number:PC28F128P30T85).
NOR Flash size is different from EVM.
So, I need to change the source code of NOR Writer and compile it, am I correct?
But I don't know which source code and which part need to be change.
Can anyone give me an advice please?
best regards,
g.f.