Other Parts Discussed in Thread: OMAP-L137
Dear all,
I have a problem with USB on OMAP-L137. I inserted a disk in USB connector and then power on the board. When the Linux are booting it prints
usb 1-1: new full speed USB device using ohci and address 2
usb 1-1: not running at top speed; connect to a high speed hub
usb 1-1: configuration #1 chosen from 1 choice
that implies Disk has been recognized BUT any device was not added to /dev folder. I checked with 1 and 4 GB disks. None of them are correct.
Please, help me on this issue.
Jone