Hi Expert
I can understand as follows from the manual, such as specification of pin B18 (VCLK/GIO79).
The following conditions:
--------------------------------------
During the reset : input(Without PD)
After reset release : VCLK
Pin internal PD does not exist
--------------------------------------
The custom board, we have 10KPU the B18 pin, but the intermediate potential was observed when it is confirmed PIN.
Because it has been input, the PD no state would otherwise, and we look forward to High resistance by PU.
It seems to operate internal PD, such as if they were present during the reset, but why do they behave like this?
Best Regards
Hidekazu