In our system we have C6455 and C6678, can I use C6678 SRIO CSL in C6645?
Thank you in advance!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In our system we have C6455 and C6678, can I use C6678 SRIO CSL in C6645?
Thank you in advance!
Xining Yu,
The C6455 and C6678 are two different TI DSPs. Its have own CSL package. I think so you can not migrate this.
CSL provide an application programming interface (API) used for configuring and controlling the DSP on-chip peripherals.
CSL for C6678:
The Chip Support Library for the 6678 device is delivered with the SYS/BIOS MultiCore SDK 2.0.
CSL for C6455:
This release of CSL for TMS320C6455 contains peripheral programming (functional and register level) APIs for C6455 modules. This set of APIs provides peripheral abstraction that can be used by higher layers of software
Please refer the below wiki article to get more details.
http://processors.wiki.ti.com/index.php/Chip_support_library