Dear Community Members,
We want to connect a USB3320 USB transceiver to the USB2/ULPI Interface and want to use linux.
There is a Swap DP/DM feature that can be accessed by setting
the respective bit in the vendor specific register 0x39(write).
We want to set it to 1 in order to prevent crossing DP/DM traces on our board.
Is this / and how is this supported by the available linux driver? Or is it
planned to be supported? Can this be configured?
Thank you for your help
Best regards
Christoph