This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x lcd

Hello friends,

I have a BBB and I just connected a 320x240 4.3" LCD to it:

5,6,5 mapping to as in many LCD "capes" for this board.
H,V sync and CLOCK.

Nothing is working :( and have no idea how to enable it. I measured the LCD CLOCK signal and has 108 MHz, obvious too high for my LCD, perhaps excellent to HDMI framer chipset.

Can I enable my LCD without re-compiling the kernel? Asking because this just taken me about 22 hours.
Has anyone some DTBS example to start with?

I use a Debian Wheezy with 3.13 kernel but the same problem on Angstrom.

Thanks very much in advance,