This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

8168 resource allocation

now i construct the link like following:

vcap---------

                       ——>merge->swms->vdis

vdec---------

i can create max 2 ch 1920*1080 dec channel initly ,the vcap can display directly

if i create 3 ch 1920*1080 ,the vcap can not be displayed,so why?

  • Share the console logs and logs of Vsys_printDetailedStatistics

  • i don't send data to the dec channel to dec,when i call Vsys_printDetailedStatistics(),

    there is nothing printf ,just following:

    0: SYSTEM: System Common Init in progress !!!
    0: SYSTEM: IPC init in progress !!!
    12: SYSTEM: CPU [DSP] syslink proc ID is [0] !!!
    12: SYSTEM: CPU [VIDEO-M3] syslink proc ID is [1] !!!
    12: SYSTEM: CPU [VPSS-M3] syslink proc ID is [2] !!!
    12: SYSTEM: CPU [HOST] syslink proc ID is [3] !!!
    12: SYSTEM: Creating MsgQ Heap [IPC_MSGQ_MSG_HEAP_3] ...
    14: SYSTEM: Creating MsgQ [HOST_MSGQ] ...
    16: SYSTEM: Creating MsgQ [HOST_ACK_MSGQ] ...
    17: SYSTEM: Opening MsgQ [DSP_MSGQ] ...
    17: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
    18: SYSTEM: Opening MsgQ [VPSS-M3_MSGQ] ...
    19: SYSTEM: Notify register to [DSP] line 0, event 15 ...
    19: SYSTEM: Notify register to [VIDEO-M3] line 0, event 15 ...
    20: SYSTEM: Notify register to [VPSS-M3] line 0, event 15 ...
    20: SYSTEM: IPC init DONE !!!
    22: SYSTEM: Creating ListMP [HOST_IPC_OUT_24] in region 0 ...
    24: SYSTEM: Creating ListMP [HOST_IPC_IN_24] in region 0 ...
    25: SYSTEM: ListElem Shared Addr = 0x40761880
    26: SYSTEM: Creating ListMP [HOST_IPC_OUT_25] in region 0 ...
    28: SYSTEM: Creating ListMP [HOST_IPC_IN_25] in region 0 ...
    29: SYSTEM: ListElem Shared Addr = 0x40796a80
    30: SYSTEM: Creating ListMP [HOST_IPC_OUT_19] in region 0 ...
    33: SYSTEM: Creating ListMP [HOST_IPC_IN_19] in region 0 ...
    34: SYSTEM: ListElem Shared Addr = 0x407cbc80
    35: SYSTEM: Creating ListMP [HOST_IPC_OUT_20] in region 0 ...
    37: SYSTEM: Creating ListMP [HOST_IPC_IN_20] in region 0 ...
    38: SYSTEM: ListElem Shared Addr = 0x4080ef80
    39: SYSTEM: Creating ListMP [HOST_IPC_OUT_21] in region 0 ...
    41: SYSTEM: Creating ListMP [HOST_IPC_IN_21] in region 0 ...
    43: SYSTEM: ListElem Shared Addr = 0x40852280
    59: SYSTEM: System Common Init Done !!!

    [host] 718: IPC_BITS_OUT : Create in progress !!!

    [host] IPC_BITSOUT:BitBuffer Alloc.ChID:0,Size:0x9E3400
    [host]
    ******* RingBuf 0 created ********

    [host] IPCBITSOUTLINK:Translated Addr Virt:0x41303080 To Phy:0x90000080
    [host]
    ###Bit buff of size from the SR # 1 : 10368000 / bufsize 2073600, maxQueueDepth 50

    [host] ###Bit buff BasePtr: 41303080 / PhyAddr 90000080

    [host] IPC_BITSOUT:BitBuffer Alloc.ChID:1,Size:0x9E3400
    [host]
    ******* RingBuf 1 created ********

    [host] IPCBITSOUTLINK:Translated Addr Virt:0x41ce6480 To Phy:0x909e3480
    [host]
    ###Bit buff of size from the SR # 1 : 10368000 / bufsize 2073600, maxQueueDepth 50

    [host] ###Bit buff BasePtr: 41CE6480 / PhyAddr 909E3480

    [host] IPC_BITSOUT:BitBuffer Alloc.ChID:2,Size:0x9E3400
    [host]
    ******* RingBuf 2 created ********

    [host] IPCBITSOUTLINK:Translated Addr Virt:0x426c9880 To Phy:0x913c6880
    [host]
    ###Bit buff of size from the SR # 1 : 10368000 / bufsize 2073600, maxQueueDepth 50

    [host] ###Bit buff BasePtr: 426C9880 / PhyAddr 913C6880

    [host] 719: IPC_BITS_OUT : Create Done !!!
    [host] HDMI Ctrl :Initializing
    [host] HDMI Ctrl :Initialized
    [host] HDMI Ctrl :Sink Connected

     

  • Run remote_debug_client and share the M3 logs

  • when i run the remote_debug_client,it has following log:

     Remote Debug Client Utility, (c) Texas Instruments 2010

    ./remote_debug_client.out <remote debug shared memory physical address in Hex>

    The shared memory physical address MUST be 4KB aligned.

  • remote_debug_client.out 0xbff00000

  • run remote_debug_client.out 0xbff00000 ,it just has following log:

    [c6xdsp ] Remote Debug Shared Memory @ 0xbff00000
    [m3video] Remote Debug Shared Memory @ 0xbff10820
    [m3vpss ] Remote Debug Shared Memory @ 0xbff21040