This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Powering of am335x with TPS650250

Hi There,

In our design we are powering AM335X with TPS650250. The RTC section of processor is powered from VLDO1. It gives 1.8V when the board is powered but that LDO is not working with RTC backup battery. Both EN_LDO pin and VIN_LDO are connected to the back up battery and main power input through a diode mechanism. Why that LDO is not working with backup battery only? 

Due to this problem i'm not getting the RTC backup.

Any help will be appreciated.

Thanks

VH