This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding the rate-match submodule for Bit Rate Coprocessor (BCP) in TI 6614 (Appleton)

Hi,

I am using BCP for PUSCH Tx (LTE) in Rate Matching module but its output data is not correct. However, when I use this module for PDSCH Tx (LTE), its output data is correct. I am wondering BCP RM only support Rate Matching for PDSCH , and   Rate Matching of PUSCH does not. If it can support both, what are differences between the BCP header config between PUSCH and PDSCH ? 

I see in the document KeyStone Architecture Bit Rate Coprocessor (BCP) User Guide of TI, however it looks it does not mention an example for Rate matching of PUSCH

Thanks,

Toan

  • Hi Toan,

    TCI66xx devices such as TCI6614 are supported directly through Local Field Applications Engineers (FAEs.)  These devices are not supported on the E2E forum.  Please contact your local FAE for support of these devices.  If you are not sure who your local FAE is, then please contact your local technical sales representative and they will be able to put you in contact with your local FAE.

    Thanks.