Other Parts Discussed in Thread: AM3354, DA8XX
Hi, All
My system is am3354 based. A splash is required in u-boot. With migrating da8xx-fb.c, the LCD hardware can be setup correctly, but failed when display splash bmp image which is read from NAND. The following are message about the error:
U-Boot SPL 2013.10 (Jan 06 2014 - 14:10:46)
The Expected Linux image was not found. Please check your NAND configuration.
Trying to start u-boot now...
U-Boot 2013.10 (Jan 06 2014 - 14:10:46)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
NAND: 256 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
rev: 0x4f201000 Resolution: 800x480 32
LCD Clock: 200000000 Divider: 6 PixClk: 33300000
Requesting 0x177000 bytes for framebuffer at 0x82000000
data abort
MAYBE you should read doc/README.arm-unaligned-accesses
pc : [<8f77bd74>] lr : [<8f77c82c>]
sp : 8f62adf8 ip : 8f651541 fp : 80813d34
r10: 84000000 r9 : 8f62af30 r8 : 4030cdcc
r7 : 4030cb7c r6 : 8f651538 r5 : 8ffbcc0c r4 : 8ffbcc10
r3 : 0000004d r2 : 00000000 r1 : 00000000 r0 : 84000000
Flags: nZCv IRQs off FIQs on Mode SVC_32
Resetting CPU ...
There are following MACROs about video display in file am335x_evm.h:
#define CONFIG_VIDEO
#if defined(CONFIG_VIDEO)
#define CONFIG_VIDEO_DA8XX
#define CONFIG_CFB_CONSOLE
#define CONFIG_VGA_AS_SINGLE_DEVICE
#define CONFIG_SPLASH_SCREEN
#define CONFIG_SPLASH_SCREEN_ALIGN
#define CONFIG_VIDEO_LOGO
#define CONFIG_VIDEO_BMP_RLE8
#define CONFIG_VIDEO_BMP_LOGO
#define CONFIG_CMD_BMP
#define DA8XX_LCD_CNTL_BASE LCD_CNTL_BASE /* am335x LCD base */
#define PWM_TICKS 0x1388
#define PWM_DUTY 0x200
#define CONFIG_SPLASH_OFFSET 0x00180000 /* for block size = 128KB, block_id = 12 */
#define CONFIG_SPLASH_ADDRESS 0x8f000000 /* the last 16MB of DDR3 (256MB) */
#endif
When u-boot startup, DENX logo can be displayed on upper-left of screen. Command clrlogo can clean that logo, but command bmp info will results the same error above.
I don't quite understand what's exactly mean of "arm-unaligned-accesses", is it related to armv7? It's highly appreciated for any suggestion and hits, thanks!
BR
Cheng Shi
emtronix