Hi
I'm using the dm8618 with the DVRRDK4.1, and I need to create NVR application.
NVR GUI application in RDK 4.1 could been tested for 8168 for receiving H.264 streams.
And I found it can be run smoothly if only have the H.264 streams , but if the IPNC contains audio, the video will be Caton!
I used the live555 in RDK 3.0 provided by udworks,It have no the problem!