Hi,
I am now using the DVRRDK4.0 in EVM8168 with a catalog daughter card. In order to capture 1 channel 1080p60 + 1 channel 720p60 video data, I managed to design a custom board to interface the VPORT by using a FPGA chip. According to the datasheet and the E2E forum, I thought that 16bit embedded BT.1120 interface is availble for DM8168 VPORT.
Thus, I got a plan:
I decide to generate some dummy video signal in BT.1120 structure by using the FPGA. In other word, FPGA is the video source; it would automatically and continueously provide dummy video data to VIP (Video in port). And I would run the Vcap + Vdis demo of DVRRDK to verify if the dummy video was captured correctly.
I doubt if this plan would work:
1. As far as I know, DVRRDK provide a driver for TVP5158s. And their I2C driver is located in M3 binary, whose source code is not provided even we have the NDA. How could we get the source code for M3 processor?
2. Besides, we only have the EVM8168 + catalog dc platform, so the Vcap + Vdis demo is not availible (no tvp5158 or composite Video in Jack in this platform) now.
3. In my plan, we don't need a video driver for FPGA, since it would automatically dump video data as soon as it powered. I don't know if the DVRRDK support a no driver control scheme, say, to capture the video directly from the VIP without any external IC configurations.
Could you help me and tell me if my plan would be feasible?
Naroah
Jan/07/2014