This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x_ICE Ethercat SyncManager watchdog

Hi,

I want to disable SyncManager Watchdog, but when I configured ESI file as following for TI_ICE Slave the TwinCAT can't operate the slave to OP Mode.

TI_ESC.xml
<Sm DefaultSize="0" StartAddress="#x1800" ControlByte="#x24" Enable="1">Outputs</Sm>

I find the ESI file of Beckhoff devices almost configured as above(ControlByte="#x24"), but this configuration is not work for TI slave.