This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

add libstdc++ to build for A8



Hi,

How / where can I add libstdc++ for the build for A8 (make -s dvr_rdk_linux)

I see that it is located in a few places

 DVRRDK_03.50.00.08/DVRRDK_03.50.00.08/ti_tools/linux_devkit/arm-none-linux-gnueabi/usr

DVRRDK_03.50.00.08/DVRRDK_03.50.00.08/ti_tools/linux_devkit/arm-none-linux-gnueabi/usr/lib/opkg

DVRRDK_03.50.00.08/DVRRDK_03.50.00.08/target/rfs_816x/usr

DVRRDK_03.50.00.08/DVRRDK_03.50.00.08/target/rfs_816x/usr/lib/ipkg

DVRRDK_03.50.00.08/DVRRDK_03.50.00.08/target/rfs_816x/usr/lib/opkg

 

which file should I edit in order to link against this library?

 

thanks,

Aaron