This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP l138 LCDK Ring IO + Qmessage concept

Hi guys,

I'm working with omap l138 LCDK for a long time and I'm facing with some conceptual misunderstanding. I'd like to combine Ring IO and QMessage handlers at the same application at DSP side.

What is the right way to do it? Am I able to create 2 tasks, one for QMessage and one for Ring IO with speficic  Server_create/delete/exec inside? I tried to proceed it in this way but QMessage interface hangs. However I'm able to use QMessage without Ring IO task...

What is the trick here? Can someone point me the solution or even provide of a code snapshot?

Thnx a lot in advance,

Dmitry