This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't chain IPIPE while capturing low resolution video

Hi,

 

We are trying  to capture a video from a source with non-standard resolution using DM365-based card.

The format of the video is UYVY and the resolution is 752X288.

The gstreamer command we are using is:

gst-launch -v v4l2src always-copy=false input-src="Camera" ! "video/x-raw-yuv, format=(fourcc)UYVY, width=(int)752, height=(int)288" ! fakesink

After running the above command, no buffers are printed to the screen.

 

IMPORTANT: We succeed to capture video with the non-standard resolution when the IPIPE is not chained.

 

We get the same issue when using Aptina sesnor (MT9M021) configured to the above non-standard resolution (We also tried other non-standard resolutions with no success).

 

1. Is it hardware issue or software (driver) issue?

2. How can we overcome this issue?

 

Regards,

Sheldon