Other Parts Discussed in Thread: TMS320DM355
Hi
I need a partial 50% transparent menu over my screen. What I have been able to do so for is a 50 % transparent menu over whole of the screen using halfhalf.attr file on frame buffer 2. Need help.
If not the complete solution, if anybody can even help me with understanding the .attr file, that would be very helpful.It has many many 3's and then many many stange Y like symbols. When opened with a binary text editor it shows 33's instead of 3's and FF's instead of the strange Y like symbols. How do they achieve 50% transparency?