This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clock setting in tcf confusion

Other Parts Discussed in Thread: OMAP3530

using CCS3.3,  OMAP3530

Im trying to understand which clocks go where in the tcf settings

Im pretty sure about the ones in the Global Settings Properties:

Board clock in KHz  = 26000  for the 26MHz on my Zoomkit

DSP Speed in MHz (clkout)  = 499.2    since thats how i set up the pll2

 

The one I'm not sure about is the one on the CLK manager properties.

Its called Input frequency. to me thats 26M, but if I uncheck the specify clock rate,

it changes to 499.2.   So Im guess thats all I really want to do.

Yes?