Other Parts Discussed in Thread: OMAPL138
Hi,
I am new working with syslink and its depending softwares.
I am trying to build syslink for running in a OMAPL137 (same ARM and DSP than OMAPL138). For that, I'm using the next sw versions:
LINUX KERNEL = 3.22.00.06
XDC Tools = 3.24.03.33
IPC=1.25.01.09
SYS/BIOS=6.33.05.46
Cross_compile_ARM=arm-2007q3
CG Tool=C6.7.4.6
After settings "products.mak" file with the corresponding parameters, I issue the command "make syslink" and I obtain the next:
gtsc@ubuntu:~/SoftwareDSP/SysLink/syslink_2_21_02_10$ make syslink-driver
#
# Making syslink-driver...
make -C packages \
DEVICE=OMAPL1XX \
GPPOS=Linux \
LOADER=COFF \
SYSLINK_REPO=/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages \
IPC_INSTALL_DIR=/opt/ti/ipc_1_25_01_09 \
CGT_ARM_PREFIX=/opt/toolchainARM/arm-2007q3/bin/arm-none-linux-gnueabi- \
LINUXKERNEL=/home/gtsc/codigoFuente/DaVinci-PSP-SDK-03.22.00.06/src/kernel/linux-davinci \
QNX_INSTALL_DIR= \
SYSLINK_BUILD_DEBUG=1 \
SYSLINK_BUILD_OPTIMIZE=0 \
SYSLINK_TRACE_ENABLE=1 \
SYSLINK_NOTIFYDRIVER=NOTIFYDRIVERSHM \
SYSLINK_TRANSPORT=TRANSPORTSHM \
syslink-driver
make[1]: Entering directory `/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages'
#
# Making syslink-driver-linux in ti/syslink/utils/hlos/knl/Linux
make -C ti/syslink/utils/hlos/knl/Linux \
ARCH=arm CROSS_COMPILE=/opt/toolchainARM/arm-2007q3/bin/arm-none-linux-gnueabi- \
KDIR=/home/gtsc/codigoFuente/DaVinci-PSP-SDK-03.22.00.06/src/kernel/linux-davinci \
SYSLINK_ROOT=/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages \
SYSLINK_PLATFORM=OMAPL1XX \
SYSLINK_PKGPATH="/opt/ti/ipc_1_25_01_09/packages;/packages;/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages" \
SYSLINK_VARIANT=OMAPL1XX SYSLINK_LOADER=COFF \
SYSLINK_BUILD_DEBUG=1 \
SYSLINK_BUILD_OPTIMIZE=0 \
SYSLINK_TRACE_ENABLE=1\
SYSLINK_NOTIFYDRIVER=NOTIFYDRIVERSHM \
SYSLINK_TRANSPORT=TRANSPORTSHM \
SYSLINK_BUILDOS=Linux
make[2]: Entering directory `/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages/ti/syslink/utils/hlos/knl/Linux'
make -C /home/gtsc/codigoFuente/DaVinci-PSP-SDK-03.22.00.06/src/kernel/linux-davinci SUBDIRS=/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages/ti/syslink/utils/hlos/knl/Linux modules
make[3]: Entering directory `/home/gtsc/codigoFuente/DaVinci-PSP-SDK-03.22.00.06/src/kernel/linux-davinci'
CC [M] /home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages/ti/syslink/utils/hlos/knl/Linux/NameServerDrv.o
/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages/ti/syslink/utils/hlos/knl/Linux/NameServerDrv.c: In function 'NameServerDrv_ioctl':
/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages/ti/syslink/utils/hlos/knl/Linux/NameServerDrv.c:342: warning: 'buf' may be used uninitialized in this function
scripts/genksyms/genksyms: 1: scripts/genksyms/genksyms: Syntax error: "(" unexpected
make[4]: *** [/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages/ti/syslink/utils/hlos/knl/Linux/NameServerDrv.o] Error 2
make[3]: *** [_module_/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages/ti/syslink/utils/hlos/knl/Linux] Error 2
make[3]: Leaving directory `/home/gtsc/codigoFuente/DaVinci-PSP-SDK-03.22.00.06/src/kernel/linux-davinci'
make[2]: *** [default] Error 2
make[2]: Leaving directory `/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages/ti/syslink/utils/hlos/knl/Linux'
make[1]: *** [syslink-driver-linux] Error 2
make[1]: Leaving directory `/home/gtsc/SoftwareDSP/SysLink/syslink_2_21_02_10/packages'
make: *** [syslink-driver] Error 2
I've tested with another version and I've checked the ".mak" file. I have not any idea about what is happening. Please, could someone help me?
Thanks