Hi,
I wanted to understand certain terminologies used in Raw Capture Progressive Mode:
a. Vertical Blanking , min = 3lines ---------- Is it same as telling it needs a minimum of 3 rows
b. Horizontal Blanking, min = 21 clk ---------- Is it same as telling it needs a minimum of 21 VP_CLK0 and 1 input clk or is it mentioned in number of rows.
c. Frame Blanking, min = 369 clk --------- ???????????????
d. Valid data period, min= 2 clk ---------- Why is it less than horizontal blanking period ? and what it is ?
Below is the timing diagram of Digital video port of OV2643
Also the master clock generated by CDCE913PW on UI board generates normal pulse of 24.0000080 Mhz
while VP_CLKIN0 and 1 are driven by 48 Mhz PCLK generated by camera module, its shape is saw tooth form.
Does the wave form shape of VP_CLKIN 0and 1 affect the VPIF ???