Other Parts Discussed in Thread: TMS320C6678
Hi all,
I'm using DSPC-8681E (which integrates four TMS320C6678 multi-core DSPs:DSP0~3) and I'm trying to run the image processing example provided in the driver package.
I'm able to follow the steps mentioned in DSPC-8681E_UserGuide.pdf for Image Processing Demonstration...until the last step: access the image processing webpage from an internet browser.
After running Image Processing loader script (image_processing.bat) the image was loaded to the DSPs successfully (It showed "load DSP image OK.") But when I opened http://192.168.1.101 on my browser, I couldn't access the multicore image processing demonstration webpage. (In stead, it showed the TCP/IP demo page.) Besides, I couldn't open http://192.168.1.102~104
I set my static IP as suggested in the users' guide (IP:192.168.1.100, subnet mask:255.255.254.0)
Both my PC and the DSP board are connected to the same switch through ethernet cables.
There's no proxy settings in the ethernet.
I can only ping 192.168.1.101 (which corresponds to DSP0) but I'm not sure if I'm actually communicating with DSP0 since http://192.168.1.101 only gives TCP/IP demo page (as mentioned before.)
I cannot ping 192.168.1.102~104 (which corresponds to DSP 1~3 respectively.)
I think the DSP hardware is working fine since I can display the PCI information of the four DSP chips in cmd window. So I guess something else is wrong in the ethernet part.
I've also tried to use different versions of driver packages (PCIE DSPC-8681E V0.79, v0.78, v0.77, v0.76, all for Windows) but none of them work.
I've been stuck for weeks and I'd be really grateful if anyone can help me with this problem. Any advice is appreciated.