Other Parts Discussed in Thread: TMS320C6678
Hi all,
I'm using DSPC-8681E (which integrates four TMS320C6678 multi-core DSPs:DSP0~3) but I encountered some problems when I'm trying to communicate between PC and DSP (DSPC-8681E_UserGuide_Win.pdf (v0.7.6) sec.5.4.
http://support.advantech.com.tw/Support/SearchResult.aspx?keyword=DSPC-8681&searchtabs=BIOS,Certificate,Datasheet,Driver,Firmware,Manual,Online%20Training,Specification,Utility,FAQ,Installation,Software%20API,Software%20API%20Manual&select_tab=Manual )
When I run ipc.bat and choose DSP #0 to load, everything works fine and I can get the same "PCIe Hello World Example, this is DSP0" reuslt as shown in the pdf.
However, if I choose DSP#1~3 to load, the results looks correct at first but ends up with errors.
The first few lines are like this:
Enter DSP ID [0~3]:3
3
Load DSP image:..\..\ipc\dsp\evmc6678l\bin\DSPC8681E\demo_evm6678l.out to 3:0, start address 0x00840000
Load DSP image OK
DDR of DSP is initialized, ready to write dummy data to DSP
dummy dummy_buffer before DSP operation:
............
But in the end it shows:
failed to wait for interrupt. Error: ERROR_TIMEOUT
I've tried to load in another .out file and run the batch file again. However the results are the same: DSP#0 works but DSP#1~3 don't.
Maybe there's something wrong with my DSP #1~3?
However, I'm able to run dsp loader and load the program into DSP memory (i.e. I'm able to query DSP information, download DSP Program Image, DSP memory read & write, Download DSP binary file, save DSP memory as a binary file) with DSP#1~3. So it seems DSP#1~3 actually work fine.
Does anyone have any idea about it? Any advice would be appreciated. Thanks.
(Btw, I'm trying to have my PC communicate with DSP directly because I've also got some problems when using ethernet too... I've posted my problems here if any of you would like to take a look:
http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/313424.aspx
Thanks again.)