This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6713 ccs3.1 with i7 processor



Hi,

i am using c6713 with ccs3.1installed in i7 processor and the 6713 drivers are installed while connecting the board the windows shows hardware is not detected 

  • Hi Mohammed,

    Thanks for your post.

    Please check whether your windows is 32-bit/64-bit OS and validate the CCS v3.1 supports the appropriate OS configuration. Also, validate the appropriate drivers used from emulator vendor.

    Please check whether the appropriate board is configured correctly in the target configuration file.

    If any of the above has mismatch, you may have the problem in launching the target connectivity in CCS.

    Could you please check the below link whether it helps?

    http://processors.wiki.ti.com/index.php/CCStudio_FAQ

    Thanks & regards,

    Sivaraj K

    ------------------------------------------------------------------------------------------------------- 
    Please click the Verify Answer button on this post if it answers your question.
    --------------------------------------------------------------------------------------------------------
     
  • Hi i am also facing the same problem while working with 6713 on I7 machine(32 Bit) and CCS3.1. The board is not detecting but when i am using i3 machine it is working fine .

    Can you please help on this as soon as possible .Let me know what settings need to be done ,