I'm trying to cross compile obp-utils (https://github.com/atmel-maxtouch/obp-utils.git) using ti-sdk-am335x-evm-06.00.00.00 in Ubuntu 10.04, but I get a libtool version mismatch error.
This is what I do:
user@ubuntu-sitara:~/atmel-maxtouch/obp-utils$source \home\user\ti-sdk-am335x-evm-06.00.00.00\linux-devkit\environment-setup
[linux-devkit]:~/atmel-maxtouch/obp-utils> ./autogen.sh --host=arm-linux-gnueabihf && make autoreconf: Entering directory `.' autoreconf: configure.ac: not using Gettext autoreconf: running: aclocal autoreconf: configure.ac: tracing autoreconf: running: libtoolize --install --copy libtoolize: putting auxiliary files in `.'. libtoolize: copying file `./config.guess' libtoolize: copying file `./config.sub' libtoolize: copying file `./install-sh' libtoolize: copying file `./ltmain.sh' libtoolize: putting macros in AC_CONFIG_MACRO_DIR, `m4'. libtoolize: copying file `m4/libtool.m4' libtoolize: copying file `m4/ltoptions.m4' libtoolize: copying file `m4/ltsugar.m4' libtoolize: copying file `m4/ltversion.m4' libtoolize: copying file `m4/lt~obsolete.m4' libtoolize: Consider adding `-I m4' to ACLOCAL_AMFLAGS in Makefile.am. autoreconf: running: /usr/bin/autoconf autoreconf: running: /usr/bin/autoheader autoreconf: running: automake --add-missing --copy --no-force configure.ac:6: installing `./missing' Makefile.am: installing `./depcomp' Makefile.am:51: variable `EXTRA_mxt_app_DEPENDENCIES' is defined but no program or Makefile.am:51: library has `EXTRA_mxt_app' as canonical name (possible typo) autoreconf: Leaving directory `.' configure: WARNING: If you wanted to set the --build type, don't use --host. If a cross compiler is detected then cross compile mode will be used. configure: loading site script /home/user/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/site-config-armv7ahf-vfp-neon-3.2-oe-linux-gnueabi checking for a BSD-compatible install... /usr/bin/install -c checking whether build environment is sane... yes checking for arm-linux-gnueabihf-strip... arm-linux-gnueabihf-strip checking for a thread-safe mkdir -p... /bin/mkdir -p checking for gawk... gawk checking whether make sets $(MAKE)... yes checking for arm-linux-gnueabihf-gcc... arm-linux-gnueabihf-gcc checking whether the C compiler works... yes checking for C compiler default output file name... a.out checking for suffix of executables... checking whether we are cross compiling... yes checking for suffix of object files... o checking whether we are using the GNU C compiler... yes checking whether arm-linux-gnueabihf-gcc accepts -g... yes checking for arm-linux-gnueabihf-gcc option to accept ISO C89... none needed checking for style of include used by make... GNU checking dependency style of arm-linux-gnueabihf-gcc... gcc3 checking build system type... i686-pc-linux-gnu checking host system type... arm-unknown-linux-gnueabihf checking for a sed that does not truncate output... /bin/sed checking for grep that handles long lines and -e... /bin/grep checking for egrep... /bin/grep -E checking for fgrep... /bin/grep -F checking for ld used by arm-linux-gnueabihf-gcc... /home/user/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/arm-linux-gnueabihf/bin/ld checking if the linker (/home/user/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/arm-linux-gnueabihf/bin/ld) is GNU ld... yes checking for BSD- or MS-compatible name lister (nm)... arm-linux-gnueabihf-nm checking the name lister (arm-linux-gnueabihf-nm) interface... BSD nm checking whether ln -s works... yes checking the maximum length of command line arguments... 1572864 checking whether the shell understands some XSI constructs... yes checking whether the shell understands "+="... yes checking for /home/user/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/arm-linux-gnueabihf/bin/ld option to reload object files... -r checking for arm-linux-gnueabihf-objdump... arm-linux-gnueabihf-objdump checking how to recognize dependent libraries... pass_all checking for arm-linux-gnueabihf-ar... arm-linux-gnueabihf-ar checking for arm-linux-gnueabihf-strip... (cached) arm-linux-gnueabihf-strip checking for arm-linux-gnueabihf-ranlib... arm-linux-gnueabihf-ranlib checking command to parse arm-linux-gnueabihf-nm output from arm-linux-gnueabihf-gcc object... ok checking how to run the C preprocessor... arm-linux-gnueabihf-gcc -E checking for ANSI C header files... (cached) yes checking for sys/types.h... (cached) yes checking for sys/stat.h... (cached) yes checking for stdlib.h... (cached) yes checking for string.h... (cached) yes checking for memory.h... (cached) yes checking for strings.h... (cached) yes checking for inttypes.h... (cached) yes checking for stdint.h... (cached) yes checking for unistd.h... (cached) yes checking for dlfcn.h... yes checking for objdir... .libs checking if arm-linux-gnueabihf-gcc supports -fno-rtti -fno-exceptions... no checking for arm-linux-gnueabihf-gcc option to produce PIC... -fPIC -DPIC checking if arm-linux-gnueabihf-gcc PIC flag -fPIC -DPIC works... yes checking if arm-linux-gnueabihf-gcc static flag -static works... yes checking if arm-linux-gnueabihf-gcc supports -c -o file.o... yes checking if arm-linux-gnueabihf-gcc supports -c -o file.o... (cached) yes checking whether the arm-linux-gnueabihf-gcc linker (/home/user/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/arm-linux-gnueabihf/bin/ld) supports shared libraries... yes checking whether -lc should be explicitly linked in... no checking dynamic linker characteristics... GNU/Linux ld.so checking how to hardcode library paths into programs... immediate checking whether stripping libraries is possible... yes checking if libtool supports shared libraries... yes checking whether to build shared libraries... yes checking whether to build static libraries... yes checking for libusb_init in -lusb-1.0... yes checking for libusb_error_name in -lusb-1.0... no checking for stdbool.h that conforms to C99... yes checking for _Bool... yes checking arpa/inet.h usability... yes checking arpa/inet.h presence... yes checking for arpa/inet.h... yes checking fcntl.h usability... yes checking fcntl.h presence... yes checking for fcntl.h... yes checking netinet/in.h usability... yes checking netinet/in.h presence... yes checking for netinet/in.h... yes checking for stdint.h... (cached) yes checking for stdlib.h... (cached) yes checking for string.h... (cached) yes checking sys/ioctl.h usability... yes checking sys/ioctl.h presence... yes checking for sys/ioctl.h... yes checking sys/socket.h usability... yes checking sys/socket.h presence... yes checking for sys/socket.h... yes checking sys/statfs.h usability... yes checking sys/statfs.h presence... yes checking for sys/statfs.h... yes checking for unistd.h... (cached) yes checking limits.h usability... yes checking limits.h presence... yes checking for limits.h... yes checking malloc.h usability... yes checking malloc.h presence... yes checking for malloc.h... yes checking netdb.h usability... yes checking netdb.h presence... yes checking for netdb.h... yes checking sys/time.h usability... yes checking sys/time.h presence... yes checking for sys/time.h... yes checking ctype.h usability... yes checking ctype.h presence... yes checking for ctype.h... yes checking for inline... inline checking for int16_t... yes checking for int8_t... yes checking for uint16_t... yes checking for uint32_t... yes checking for uint8_t... yes checking for size_t... yes checking for stdlib.h... (cached) yes checking for GNU libc compatible malloc... (cached) yes checking for stdlib.h... (cached) yes checking for GNU libc compatible realloc... (cached) yes checking for bzero... yes checking for gettimeofday... yes checking for select... yes checking for setlocale... yes checking for socket... yes checking for strerror... (cached) yes checking for strncasecmp... yes checking for tolower... yes configure: creating ./config.status config.status: creating Makefile config.status: creating doc/Makefile config.status: creating config.h config.status: executing depfiles commands config.status: executing libtool commands make --no-print-directory all-am /bin/bash ./libtool --tag=CC --mode=compile arm-linux-gnueabihf-gcc -DHAVE_CONFIG_H -I. -march=armv7-a -marm -mthumb-interwork -mfloat-abi=hard -mfpu=neon -mtune=cortex-a8 --sysroot=/home/user/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/armv7ahf-vfp-neon-3.2-oe-linux-gnueabi -I./src -fvisibility=hidden -ffunction-sections -fdata-sections -g -Wall -Wmissing-declarations -Wmissing-prototypes -Wnested-externs -Wpointer-arith -Wsign-compare -Wchar-subscripts -Wstrict-prototypes -Wwrite-strings -Wshadow -Wformat-security -Wtype-limits -Werror -D__GIT_VERSION=\"1.15-30-gf072\" -U_FORTIFY_SOURCE -D_FORTIFY_SOURCE=0 -DHAVE_LIBUSB -march=armv7-a -marm -mthumb-interwork -mfloat-abi=hard -mfpu=neon -mtune=cortex-a8 --sysroot=/home/user/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/armv7ahf-vfp-neon-3.2-oe-linux-gnueabi -MT libmaxtouch.lo -MD -MP -MF .deps/libmaxtouch.Tpo -c -o libmaxtouch.lo `test -f 'src/libmaxtouch/libmaxtouch.c' || echo './'`src/libmaxtouch/libmaxtouch.c libtool: Version mismatch error. This is libtool 2.4.2, but the libtool: definition of this LT_INIT comes from libtool 2.2.6b. libtool: You should recreate aclocal.m4 with macros from libtool 2.4.2 libtool: and run autoconf again. make[1]: *** [libmaxtouch.lo] Error 63 make: *** [all] Error 2
/usr/bin/libtoolize and /usr/bin/libtool are version 2.2.6b
/home/user/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/bin/libtoolize and
/home/user/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/bin/i686-arago-linux-libtool are version 2.4.2
How to cross compile it with success?, should I install Ubuntu 12.04 wich includes libtool 2.4.2?
My Qt application is compiled in the same environment and it runs fine on my AM3358 board.
Thank you in advance