This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Completely restoring factory defaults

Hi

I am working on a DM6446 development board, but am seriously struggling to get things going...again.  I got the board after someone else worked on it, but now no-one seems to be able to get things going anymore.  I have downloaded all the recent software, and suspect that there are some serious version mismatches and corrupt files somewhere in the system.  What I would like to know is how I can completely restore the factory defaults on the development board, so that it becomes like a newly shipped one.  If I can do that, then I'll be able to follow the GSG and hopefully get the card going as soon as possible.  This is the only way I can think of to get the development board into a state where I can actually start developing programs, as I've tried many times to get things going but got stuck in the endless amount of error messages I got.

Regards

Andre