This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OpenMax Test Bench - What is it for?

Expert 1130 points


What is the purpose of the OpenMax Test Bench? Can I use it to test the H.264 encoder?

I need to do multiple encodings of yuv source file, change the encoder parameters for each test and save the encoded h264 file. Someone told me I can do this with omtb.

  • Hello,

    MRI said:
    What is the purpose of the OpenMax Test Bench?

    OMTB or OpenMAX Test Bench is a software application that can be used to create and connect instances of TI supported Multi-media Software Modules*, configure them and run them together as an intended use-case.

    Yo could check OMTB user guide for more information. You could find it in:

    /ti-ezsdk_dm814x-evm_5_05_02_00/example-applications/omtb_01_00_01_07/packages/ti/sdo/omtb/docs

    Best Regards,

    Margarita