I designed my custom board that refer to MS_TI_DM814x_BB_REVD_SCH in MISTRAL. And I changed PHY chip (88e1111). When linux boots up, the net does not work.
Anyone help me please, What should I do?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I designed my custom board that refer to MS_TI_DM814x_BB_REVD_SCH in MISTRAL. And I changed PHY chip (88e1111). When linux boots up, the net does not work.
Anyone help me please, What should I do?
Hi Pcxmathy,
Have you gone through the below wiki page?
http://processors.wiki.ti.com/index.php/TI81xx_PSP_Porting_Guide#Ethernet_Driver_-_Adding_Custom_Ethernet_Phy
Check also silicon errata advisories:
Advisory 3.0.21 Boot: Gigabit Ethernet Boot Will Not Work Reliably
Advisory 3.0.29 Boot: Ethernet Boot ROM Code PHY Link Speed Detection
Advisory 3.0.30 Boot: Ethernet Boot ROM Code Sends an Incorrect Vendor Class Identifier in BOOTP Packet
Advisory 3.0.85 EMAC and Switch Subsystem: Reset Isolation Feature is Not Supported
Best regards,
Pavel